Technical FAQs

Ask a Question

How do the cables come in to a 5/15kV HVL load break interrupter switch. Are there bus extensions available to connect to existing bottom entry cables?

The standard upright switch has line terminals near the top of the enclosure and toward the front. Larger cables will require a rear connector assembly to avoid bending toward the front of the switch. If there are existing cables in the floor, the rear connector assembly can be modified at the factory to meet the requirements.

CTA-ID : 2032286
Was this helpful?
What can we do to improve the information ?