Technical FAQs

Ask a Question

How is the locking wire of a S44936 toggle padlocking device fastened to a MGA36600?<br />

It is part of the sealing hardware for the breaker cover. The cover is sealed to show evidence of tampering if removed while the removeable handle padlock attachment is applied. Refer to the supplied instruction bulleting for complete information.


CTA-ID : 2032255
Was this helpful?
What can we do to improve the information ?