Technical FAQs

Ask a Question

What are the BTU ratings for ATS48`s from 50-500 HP, 230Vac and 460Vac units?

1 watt is approximately 3.41 BTU/h
1000 BTU/h is approximately 293 W
1 horsepower is approximately 2540 BTU/h
With the WATT or HP data available in the catalog, BTU for all products can be calculated.

CTA-ID : 2032344
Was this helpful?
What can we do to improve the information ?