Technical FAQs

Ask a Question

Is the Protected LED lamp only for a ZB4 or ZB5 available?

Issue:
Is the Protected LED lamp only for a ZB4 or ZB5 available?

Product Line:
22mm Push Buttons

Environment:
ZB4/ZB5 22mm Push Buttons

Cause:
Clarify if the entire light module needs to be replaced or just the lamp.                      

Resolution:                                                                 
The LED in the Protected LED units are not replaceable.
 
Was this helpful?
What can we do to improve the information ?