Technical FAQs

Ask a Question

Where is the UL label on the HVMB305200 MiniBreak switch?

The labels are on the back pan, not the front. If UL labels are not there, they can not be sent out and cannot be put on in field. They must be sent back to Smyrna to be put on.

CTA-ID : 2032370
Was this helpful?
What can we do to improve the information ?