Technical FAQs

Ask a Question

What thicknesses of GPO-3 red glass polyester are available from the Smyrna Plant?

Smyrna does not stock GPO-3 red glass polyester anymore. The parts using this material are outsourced. This material can be ordered .031``, .125``, .188`` or 0.25`` thick.


CTA-ID : 2032280
Was this helpful?
What can we do to improve the information ?