Technical FAQs

Ask a Question

Is the head rotatable on an XCSE Safety Interlock Switch?

Yes, the head can be rotated through 360 degrees in 90 degree steps by loosening the screw on the front (just below the head on the right) of the Safety Interlock Switch.

CTA-ID : 2032251
Was this helpful?
What can we do to improve the information ?