Technical FAQs

Ask a Question

Can you add tenant breaker(s) to the two gang UT2R1121B meter unit?

This unit is not designed to accept tenant breaker(s). Individually enclosed circuit breakers will have to mounted separately in conjunction with this device.


CTA-ID : 2032205
Was this helpful?
What can we do to improve the information ?