Technical FAQs

Ask a Question

What is the size of the standard pipe thread that comes on the pressure fitting of a 9012GAW2 pressure switch?

The standard pipe thread on the fitting is 1/4-18 NPTF type, per page 10 of catalog number 9012CT9701.

CTA-ID : 2032262
Was this helpful?
What can we do to improve the information ?