Technical FAQs

Ask a Question

Can a single section indoor HVL/cc switch have cables in and out the top?

Not with the basic standard switch. The switch bottle goes completely from the front to back of the enclosure. In order to have cables enter and exit from the same section, a rear extension must be added to the back of the enclosure. The standard depths of rear extensions are 16.75``, 24.00`` and 30.00``.
The depth of the extension depends on the size of the cables.

CTA-ID : 2032351
Was this helpful?
What can we do to improve the information ?