Technical FAQs

Ask a Question

Can AL100FA type lugs be factory installed on a FAL3603013T circuit breaker?

These are mining duty rated breakers, and come with the AL50FA lug on them. AL100FA lugs can be field installed, or factory installed using suffix 5853 for high ampere AL100FA type lugs. Complete part number is FAL3603013T5858.


CTA-ID : 2032149
Was this helpful?
What can we do to improve the information ?