Technical FAQs

Ask a Question

Can the 1200A PAF2036 circuit breaker in a EZM31200CB EZ Meter-Pak Main Breaker device be converted to an alternate ampere rating?

Product Application

Product Line:
EZM Metering

Alternate main amperage ratings

The PAF2036 circuit breaker frame provided in the EZM31200CB is supplied with PA31200RC rating columns. The PA31200RC rating columns can be removed and replaced with alternate, lower ampere rated, rating columns:
For 600A ampere rating, use PA3600RC
For 700A ampere rating, use PA3700RC
For 800A ampere rating, use PA3800RC
For 1000A ampere rating, use PA31000RC

CTA-ID : 2032158
Was this helpful?
What can we do to improve the information ?