Technical FAQs

Ask a Question

On Circuit Breaker catalog number KAL926225, what is the meaning of the ``9`` in the catalog number? Does it have copper lugs?

Yes. The ``9`` in the catalog number indicates that the breaker is marine duty rated. The Marine rating on a K frame breaker requires copper lugs.


CTA-ID : 2032136
Was this helpful?
What can we do to improve the information ?