Technical FAQs

Ask a Question

What type of lug is used with a circuit breaker catalog number MAL36800? What is the lug wire range?

The MAL36800 breaker uses an AL900MA lug which will accomodate (3) #3/0 AWG-500 kcmil conductors.


CTA-ID : 2032135
Was this helpful?
What can we do to improve the information ?