Technical FAQs

Ask a Question

Can the QO or HOM Homeline arc fault breaker AFI be used with knob and tube wiring?

Yes. As long as there is not a shared neutral and the neutral is grounded at the service entrance only.



CTA-ID : 2032318
Was this helpful?
What can we do to improve the information ?