Technical FAQs

Ask a Question

Does Square D require or recommend any taping at the end of feeder cables attached to bus bar? This applies to metal enclosed switchgear at 5kV and 15kV with stress cones on the cables/

Square D does not recommend any unless it is a job that requires insulated bus.


CTA-ID : 2032283
Was this helpful?
What can we do to improve the information ?