Technical FAQs

Ask a Question

Is a 2000A main circuit breaker available in the EZ Meter-Pak product line?

Yes, we do offer a 2000A main circuit breaker. For use on single phase services, we can offer EZM12000CB or EZM12000CBU. For use on three phase services, we can offer EZM32000CB or EZM32000CBU. In all cases, 240Vac maximum is applicable.

CTA-ID : 2032267
Was this helpful?
What can we do to improve the information ?