Technical FAQs

Ask a Question

Can auxiliary load terminals be added in the field to 8536 Size 00, 0, 1 and 2 Starters with ``bimetallic overload relays``?

The only way to add auxiliary load terminals in the field to Size 00, 0, 1 and 2 Starters is to change the overload relay to one that has the auxiliary load terminals installed on it. 9065SDTO6B has auxiliary load terminals and can replace the 9065SDO6B or 9065SDTO6B2 has auxiliary load terminals and can replace the 9065SDO6B2.


CTA-ID : 2032092
Was this helpful?
What can we do to improve the information ?