Technical FAQs

Ask a Question

Can Aluminum conductors be used on a Q frame Powerpact breaker such as QB, QD, QG, QJ, rated at 250A?

Q frame Powerpact breakers such as QB, QD, QG, QJ, rated at 250A are permitted to use copper conductors only. See page 6 of Document 0734CT0201.


CTA-ID : 2032097
Was this helpful?
What can we do to improve the information ?