Technical FAQs

Ask a Question

Can auxiliary load terminals be added in the field to 8536 Size 00, 0, 1 and 2 Starters with ``solid state overload relays``?

Use the 9999PFL kit to add auxiliary terminals to Size 00, 0, 1 and 2 Starters with solid state overload relays.


CTA-ID : 2032093
Was this helpful?
What can we do to improve the information ?