Technical FAQs

Ask a Question

What is the most common TVSS unit installed internal to our NQOD factory assembled panelboards?

It would be the Square D SurgeLogic TVS2IMA16P (P = Peru Interplant only). The unit is rated 208Y/120VAC 3 phase 4 wire and has protection modes of 160KA per phase.

CTA-ID : 2032137
Was this helpful?
What can we do to improve the information ?