Technical FAQs

Ask a Question

Can auxiliary load terminals be added in the field to 8536 Size 00, 0, 1 and 2 Starters with ``melting alloy overload relays``?

The only way to add auxiliary load terminals in the field to Size 00, 0, 1 and 2 Starters is to change the overload relay to one that has the auxiliary load terminals installed on it. 9065SDTO5 has auxiliary load terminals and can replace the 9065SDO5 or 9065SDTO8 has auxiliary load terminals and can replace the 9065SDO8.


CTA-ID : 2032091
Was this helpful?
What can we do to improve the information ?