Technical FAQs

Ask a Question

What are WL1 and WL3 Masterpact NW breakers, and what is the difference between them? The WL1 and WL3 are not found in any literature.<br />

WL1 and WL3 are descriptions in Quote to Cash given to the UL listed Masterpact NW ``W`` frame breaker labeled with the Squared D brand. A ``1`` in the third catalog number position is the N interrupting rating of 65kA at 480Vac. A ``3`` in that position is the H interrupting rating of 100kA at 480Vac.

CTA-ID : 2031287
Was this helpful?
What can we do to improve the information ?