Technical FAQs

Ask a Question

Can a second 200 ampere main service disconnect be added to the CU12L400FB?

Yes, it can. Additional space is provided for the field installation of a second QDL main service disconnect, 200A maximum. Further additional space is provided for the field installation of up to four QOH main service disconnects, 125A maximum. The total ampacity of the combination of QOH breakers cannot exceed 200A.


CTA-ID : 2030647
Was this helpful?
What can we do to improve the information ?