Technical FAQs

Ask a Question

Can a second 200 ampere main service disconnect be added to the RU3040D400CL?

Yes, it can. Additional space is provided for the field installation of a second QDL main service disconnect, 200A maximum.


CTA-ID : 2030666
Was this helpful?
What can we do to improve the information ?