Technical FAQs

Ask a Question

Can a second 200 ampere main service disconnect be added to the SU3040D300CB?

Issue:
Product design features

Product Line:
Combination Service Entrance Devices

Environment:
Service Disconnects

Cause:
Application

Resolution:
No, the device is rated 300amp MAX. and it comes from the factory with one 200amp service disconnect installed. The additional space provided for the second field installation QDL main service disconnect, is limited to 100A maximum.


CTA-ID : 2030661
Was this helpful?
What can we do to improve the information ?