Technical FAQs

Ask a Question

Is there a replacement for an SED361600LS breaker? It shows obsolete in Q2C.

Use a catalog number of an SED363000LS breaker and an ARP067 rating plug, with the long time setting set to .80. This is a 3000A breaker with a rating plug and setting that brings its total amperage down to 1600A.


CTA-ID : 2031161
Was this helpful?
What can we do to improve the information ?