Technical FAQs

Ask a Question

Is there an insulating kit for the PK32DGTA ground bar?

Issue:
Selection

Product Line:
Panel board accessory

Cause:
Selection

Resolution:
The ground bar isolating kit PKGTAB is only suitable for use with the PK7GTA thru the PK23GTA equipment ground bars. It is not suitable for use on the PK32DGTA. 



CTA-ID : 2030678
Was this helpful?
What can we do to improve the information ?