Technical FAQs

Ask a Question

Can transformers containing mineral oil fluid be retro filled with a high fire point seed based fluid?

Mineral oil filled transformer can be retro filled with either of the two available seed based fluids. The fluids are FR3 manufactured by Cooper Industries and Bio-Temp manufactured by ABB Inc. Instructions for the fluid conversion are available from the Medium Voltage TAG group in Nashville.

CTA-ID : 2031117
Was this helpful?
What can we do to improve the information ?