Technical FAQs

Ask a Question

What is the replacement for an HCW1444-4 I-Line panelboard interior?

Use an HCP14504. It has the same amount of branch mounting space and will fit in the old 44" high box. However, the original trim will not fit and there is no replacement trim available.
Was this helpful?
What can we do to improve the information ?