Technical FAQs

Ask a Question

Does anyone have any data or information on EMF/RFI measurements on switchgear?

It is not needed to test a complete lineup, but just any components with electronics related. The SEL351 relay and the CM4000 circuit monitor passed the tests. MIL-STD-461E is the EMI susceptibility and emissions testing standard.

CTA-ID : 2030990
Was this helpful?
What can we do to improve the information ?