Technical FAQs

Ask a Question

How do you select thermal units for the Class 8536 Type SH Series B controller ?

Select with the same tables as the Series A Size 6 starter. Note that the bimetallic and melting alloy overloads incorporate a 800:5 CT.


CTA-ID : 2031110
Was this helpful?
What can we do to improve the information ?