Technical FAQs

Ask a Question

What are the repair parts for an EZML312400, Series M01 branch unit?

Only the parts listed below are considered field replaceable:

Customer Cover (includes labels) - EZML312400C
Blank Covers (includes 3 covers) - EZML400BK2
Cover Screws - 4020513002K
Meter Socket Cover (cover for one meter position) - EZMCRC
Parts Kit (one position, meter socket line side through tenant breaker base) - EZML1400KIT
Replacement Tenant Circuit Breaker (one position) - LAL26400
Circuit Breaker RB Cover (one position) - BCM
Enclosure connecting hardware and Service Disconnect labels - 7329791750
Mounting Channel - 7329776601
Equipment Ground Bar Assembly
Ground Bar - 7329644550
Ground Bar Mounting Screws - (2) 2153271761
End Closing Cap Kit - EZMCAP
End Closing Cap Kit (Right Side Only Shallow) - EZMSCAP


CTA-ID : 2031093
Was this helpful?
What can we do to improve the information ?