Technical FAQs

Ask a Question

How is an external 24vdc power supply connected when used to power the logic inputs on the Altivar ATV66 drive?

Need to connect the external 24vdc power supplies negative (-) or common wire to the COM terminal of the ATV66 drive, the power supplies positive (+) wire would then connect to the ATV66 logic inputs through a dry contact closure.


CTA-ID : 6978
Was this helpful?
What can we do to improve the information ?