Technical FAQs

Ask a Question

Can an EZM Ring type without bypass branch device, be converted to a EZML Ringless type with lever bypass branch device?

Issue:
Product Design features

Product Line:
EZM metering equipment

Environment:
Meter socket conversion

Cause:
Utility approval

Resolution:
No, the EZM Ring type without bypass CANNOT be converted to the EZML Ringless with Lever Bypass. The EZML device MUST be purchased directly.


CTA-ID : 2031107
Was this helpful?
What can we do to improve the information ?