Technical FAQs

Ask a Question

What is the part # of the field installable alarm contacts module for the Powerpact H & J frame breakers?

Use an SD29450 for a 6 A max standard module and a S29452 for a low level 1 mA min module. Either would fit into the ``SD`` ( alarm switch ) cavity in the breaker ( to the immediate left of the toggle) .


CTA-ID : 2031034
Was this helpful?
What can we do to improve the information ?