Technical FAQs

Ask a Question

Can a second 200 ampere main service disconnect be added to the CU816D400FB?

Yes, it can. Additional space is provided for the field installation of a second QDL main service disconnect, 200A maximum.

CTA-ID : 2030654
Was this helpful?
What can we do to improve the information ?