Technical FAQs

Ask a Question

Is the ANSI Masterpact NW 3200amp L1 (200kA AIR) breaker a W or Y frame?

It is a Y frame, 6 pole breaker.
Note:
W-frame (Standard Construction)
Y-frame (Wide Construction)


CTA-ID : 2031024
Was this helpful?
What can we do to improve the information ?