Technical FAQs

Ask a Question

What is the operating range of the 1027, 24 Vdc shunt trip.

It requires 75% or more of the rated voltage.


CTA-ID : 2030995
Was this helpful?
What can we do to improve the information ?