Technical FAQs

Ask a Question

Is the RC816D200CH provided with a factory installed service disconnect?

Yes, a HOM2200 is supplied factory installed. The factory installed HOM2200 feeds the 8 space/16 circuit loadcenter interior. Additional space is provided for the field installation of a second HOM main breaker, 50A maximum.


CTA-ID : 2030614
Was this helpful?
What can we do to improve the information ?