Technical FAQs

Ask a Question

Is the SC816D200C provided with a factory installed service disconnect?

Product Features

Product Line:

Clarifying if a main breaker service disconnect is provided.

Yes, a HOM2200 is supplied as a back fed main breaker service disconnect, factory installed. The HOM2200 feeds the 8 space/16 circuit loadcenter interior. Additional space is provided for the field installation of a second HOM main breaker service disconnect, 50A maximum.

CTA-ID : 2030613
Was this helpful?
What can we do to improve the information ?