Technical FAQs

Ask a Question

XUVK0252VS or XUVK0252S: Does it need a cable and if so what is the part number?<br /><br />

These devices require a 4-pin M8 quick connect cable. Use XSZCS141 for 2m long cable with straight connector and XSZCS151 for a 2m long cable with a 90 degree connector.



CTA-ID : 2030918
Was this helpful?
What can we do to improve the information ?