Technical FAQs

Ask a Question

I am assembling some NEMA 3R raintight type wireway in 90 degree configuration. Do I have to buy two male sections and a 90 degree elbow to make the bend? What parts do I need to put these together?

Issue:
Parts needed

Product Line:
Wireway

Environment:
Nema 3R Raintight

Cause:
Application

Resolution:
You must order one male section, one female section, and an extra connector to complete the 90 degree connection.


CTA-ID : 2030720

Was this helpful?
What can we do to improve the information ?