Technical FAQs

Ask a Question

Is there a way to bypass or eliminate the tenant breakers in MP metering equipment? Customer is feeding main breaker load centers from the meters directly.

No. There is no provision for bypassing the tenant breakers in MP Metering equipment. The devices are UL listed for use with circuit breakers. In addition, bypassing the tenant circuit breakers violates the National Electric Code regarding Service Equipment applications, which requires that the equipment constitute the main control and cutoff of the supply.


CTA-ID : 2030748
Was this helpful?
What can we do to improve the information ?