Technical FAQs

Ask a Question

On a MPL53225 or MPL64225 are alternate lugs available to accept 750 KCMIL wire?

Issue:
Application

Product Line:
MP Meter-Pak

Cause:
Alternate lugs

Resolution:
Yes, this can be done. Remove the existing phase and neutral lugs, and install the MMSK4 lug landing pad with mounting hardware. Order lugs separately. Examples: ILSCO part number TA8002N or Anderson part number L1D2800, which both accept 1 # 300-800 KCMIL AL or CU cable. The MMSK4 kit will accept two (2) lugs per phase and neutral. 
NOTE: This alternate lug detail is not applicable to the MPL32225. 



CTA-ID : 2030740
Was this helpful?
What can we do to improve the information ?