Technical FAQs

Ask a Question

Is the SC12L200S provided with a factory installed service disconnect?

Issue:  
What 200 A breaker can I install in my SC12L200S CSED?

Product line:  
Combination service entrance disconnects

Environment:  
Homeline CSED Meter Main devices

Resolution:  
No, the service disconnect(s) must be field installed in this device.  Install only HOM type of breaker, 15-110A and/or a 150-200A breaker maximum.  A 125A breaker cannot be used.  A maximum of (6) 15-110A HOM breakers can be installed.  A maximum of (1) 150-200A HOM breaker can be installed. If a 150-200A HOM breaker is installed, a maximum of (4) 15-110A HOM breakers can be installed.
Was this helpful?
What can we do to improve the information ?