Technical FAQs

Ask a Question

Are LA400S or a LA400DS available with special paint?

Not available on Stainless Steel device.
The NEMA 1 is available however there is a minimum quantity of 5 that must be ordered. See page Supplementary Digest for more details.

CTA-ID : 2030698
Was this helpful?
What can we do to improve the information ?