Technical FAQs

Ask a Question

What components are used in an FHE36000A?

The FHE36000A consists of a FHL36000M molded case switch factory installed in a (modified) FA100A enclosure. The enclosure markings are modified to indicate that the device is an enclosed molded case switch, not an enclosed circuit breaker.

CTA-ID : 2030850
Was this helpful?
What can we do to improve the information ?