Technical FAQs

Ask a Question

What are the dimensions for the padlock attachment ZB4BZ6* ?

Issue::
What are the dimensions for the padlock attachment ZB4BZ6*

Product Line:
22mm Push Buttons

Environment:
XB4/XB5 22mm Push Button

Cause:
Dimensions are needed for application.                                                

Resolution:
Wide 43mm X Height 45mm X Depth 26mm (flip closed) 45mm (flip open)



 
Was this helpful?
What can we do to improve the information ?