Technical FAQs

Ask a Question

Is the RC12L200C provided with a factory installed service disconnect?

No, the service disconnect(s) must be field installed in this device. Install only HOM type of breaker, 15-100A and/or a 150-200A breaker maximum. A 110A or 125A breaker cannot be used. A maximum of (6) 15-100A HOM breakers can be installed. A maximum of (1) 150-200A HOM breaker can be installed. If a 150-200A HOM breaker is installed, a maximum of (4) 15-100A HOM breakers can be installed.


CTA-ID : 2030588
Was this helpful?
What can we do to improve the information ?